Edit an image

Edit an image on the canvas to edit the picture that appears in the image object.
  1. From
    Project view
    , double-click
    MainWindow (type)
    to open the editor in a separate tab.
  2. On the canvas, double-click the image you want to change.
    NOTE: You can also edit an image from
    Project view
    by double-clicking the image in
    Project view
    to open a tab in the editor.
  3. In
    Select file
    , select the image to display and then choose
    Select
    .
    TIP: If the image does not appear in
    Select file
    , select
    Import file(s)
    and in
    Import file(s)
    , select the image to import and then choose
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal