Add a scale line pen

Add a scale line pen to visualize the distance between two variable values.
Prerequisites
  1. To add a scale line pen
  2. Create two variables of the Number data type.
    For more information, see Variables.
  3. In
    Properties
    , next to
    Pens
    , select
    Add
    and select
    Scale line pen
    .
  4. Create dynamic links between the
    X
    and
    Y
    properties and the variables.
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal