Create a thermometer linear gauge

Create a linear gage with a warning zone that indicates the current temperature.
  1. Create and configure the gauge:
    1. Right-click
      MainWindow (Type)
      and select
      New
      Base controls
      Linear gauge
      .
    2. Hover-over a gauge, select
      Edit
      , and enter
      ThermometerGauge
      .
    3. In
      Properties
      , create a dynamic link between
      Value
      and
      ProjectName
      Model
      TemperatureAlarmVariable
      .
      For more information about dynamic links, see Create dynamic links.
  2. Set the value gauge warning zone:
    1. In
      Properties
      , next to
      Warning zones
      , select
      Add
      .
    2. Under
      WarningZone1
      , set
      Color
      to
      #f30000
      .
    3. Set
      From
      to
      75
      .
    4. Set
      To
        to
      100
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal