Import Companion Specifications
    Add support for more Companion Specifications to 
FactoryTalk Optix Studio
.Prerequisites
- Obtain anXMLfile with Companion Specifications to import.
- CloseFactoryTalk Optix Studio
- To import Companion Specifications
- Copy theXMLfile with Companion Specifications toC:\Program Files\Rockwell Automation\FactoryTalk Optix\Studio\CompanionSpecifications
- If prompted, selectContinue.
The imported Companion Specifications are available in 
FactoryTalk Optix Studio
.Provide Feedback