- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Connections tab
Use the
Connections
tab to connect a parameter in a program to another parameter in the same or different program, controller parameters and tags, or device tags. Do this to pass data into and out of the program, controller, or device. To open the
Connections
tab, select 
System
and right-click a program or select 
Execution
and right-click a program with a controller, select View tags and parameters
to select a parameter, and then in Properties
, select Connections
.Provide Feedback