- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Change controller properties
Use the settings in
between viewing the controller properties in the offline workstation
and the online workstation
.
Properties
to change the controller name and description. When online with the controller, you can toggle 


- On the explorer bar, selectDevices.
- InDevices, select the controller.
- IfPropertiesis not open, on the pane bar, selectProperties.
- InProperties, underGeneral, change:
- Name. The unique name of the controller.TIP: Controller names:
- Can contain up to 40 valid characters.
- Can contain only alphanumeric characters and underscores
- Must begin with a letter or an underscore
- Cannot contain consecutive underscores
- Must end with a character other than an underscore
- Can be edited only when offline with the controller.
- Description. The description of the purpose of the controller in the system.
Provide Feedback