- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Create a definition from a modified instance
Follow these steps to create a definition from a modified instance.
IMPORTANT:
Modifying FactoryTalk Smart Objects using the Code Editor may result in syntax errors that will prevent the explorers from displaying information. We recommend using the user interface to create or modify FactoryTalk Smart Objects.
- On the explorer bar, selectSystem.
- Right-click aFactoryTalk Smart Objectand selectAdd to Library.
- InNew, complete:FactoryTalk Smart Objectdefinition
- Name. A name for the definition.
- Description. An optional description for the definition.
- Version number. The version number is XXX.YYY.ZZZ where each segment can be 0...999.
- SelectCreate.
Provide Feedback