- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Add a shared project to the FactoryTalk Vault
Add a shared project to the FactoryTalk Vault solution to provide a centralized solution to securely store documents, manage data access, and collaborate on projects. This will help you remain in sync with your team. If FactoryTalk Vault is not available during project creation, your shared projects may not be stored in the FactoryTalk Vault yet. You can use the Push option to add a shared project to a FactoryTalk Vault solution.
- In theAdd Project to Vault Solutiondialog box, select one of these options for a FactoryTalk Vault solution:
- Select from exiting solutions
- Create solution
- SelectAdd to solutionto place your project in the chosen FactoryTalk Vault solution and push the files.
Provide Feedback