- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
connections object
Defines the device connections topology of a set of connected devices. The topology models the parent-child relationship among devices.
connections [rootDevice]{ path [bus] { <device> { path [bus] { <device> ... } ... } ... } ... }
Property | Description |
---|---|
rootDevice (required) | Device originating the connections tree. |
bus (required) | Defines the route from the originator device to each of the targets. |
device | Child device of a parent device connected through the upstream path. |
Provide Feedback