- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
File name extensions
File names in the Domain Specific Language (DSL) use these extensions:
File name extension | File type |
.s5kproj | Projects. Contains the project ID and version. |
.logix | Files related to control, such as controller application, program, routine, AOIs, and tasks. |
.smo | Smart objects. |
.model | Area models. |
Provide Feedback