timeSynch object

timeSynch object

Defines the time sync properties. This object is applicable for controllers only.
timeSync.<property name> := <property value>
Property
Description
enabled
Indicates time synchronization is enabled.
priorityOne
The relative first priority of the grandmaster clock and local clock to other clocks in the system. The priority range is 0 - 255. The highest priority is 0. The default is 128.
priorityTwo
The relative second priority of the grandmaster clock and local clock to other clocks in the system. The priority range is 0 - 255. The highest priority is 0. The default is 128.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal