Controller example

Controller example

This example shows the code for a device defined as a controller.
ControllerDevice _1756_L85E Controller1 { catalogNumber := "1756-L85E"; productCode := 168 majorRev := 34; minorRev := 1; moduleEKeyingState := "DISABLED"; port RA1756 port1 { cipPortId := "1"; address := "0"; } port Ethernet port2 { cipPortId := "2"; ethernetLinkInstance1 := 1; address := "1.1.1.2"; } physicalPort Ethernet A1 { enabled := true
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal