- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Guidelines for routines in Add-On Instructions
Follow these guidelines when defining routines in an add-on instruction (AOI).
- Routines must be named according to what they represent. Name a logic routine Logic(), and name a prescan routine prescan().
- Routines within add-on instructions cannot have parameters nor routine-scoped tags. Tags can only be defined in the AOI.
- Routines within an AOI cannot have parameters even through the parentheses () are required for the routine declaration.
- Routines within an AOI cannot contain routine-scoped tags. Tags can only be declared within the AOI itself.
- You can declare a routine outside of the AOI in the same file or in another file.
- To declare a routine as external to the AOI, add theexternkeyword before theroutinekeyword.
- External routines have two parts:
- The declaration of the external routine within the AOI. For example:
- The routine implementation itself. For example:
extern routine [name] ();[aoi name].[routine name] () {< content>}
Provide Feedback