Add-On Instruction attributes

Add-On Instruction attributes

This table describes add-on instruction attributes.
Attribute
Description
Name
The name of the add-on instruction component.
Version
The revision of the add-on instruction, in the form of MajorRevision.MinorRevision. Each revision number can be 1 to 999. If there is no period, the number is treated as a major revision only.
RevisionExtension
Additional information about the revision, with a maximum of 40 characters.
note
Information about the revision, with a maximum of 128 characters.
Vendor
The name of the add-on instruction vendor, with a maximum of 40 characters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal