Calibration view parameters
The
Calibration
view includes these parameters:Parameter | Description |
---|---|
Channel | Displays the channel number to which this configuration applies. |
Calibration Range | Shows the value currently configured for the channel. Values display according to the Input Type selected:
|
Calibration Gain | Shows the calibration gain value as reported by the device. |
Offset | Shows the offset in units (mA, ohms, mV or V) as reported by the device. |
Last Calibration Date | Shows the last calibration date for the channel. The time and date listed here is based on the time on the computer running the application. |
Calibration Status | Shows the status of the calibration per channel as the calibration occurs. Valid values include:
|
Start Calibration | Select to begin the calibration process. Start Calibration is enabled when the device is inhibited, online with the controller, and at least one channel is selected to start the calibration process. |
Provide Feedback