Calibration mismatch

Performing calibration might cause unexpected results if:
  • At least one channel is selected, and
  • There is a mismatch between the device in the application's I/O configuration and the actual physical device, and
  • The system is active.
We recommend that you select
No
, check your configuration, and shut down your system before performing calibration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal