Configure alarm properties

Configure alarm properties to alert you when the device exceeds configured high or low limits.
To configure alarm properties
  1. On the tab for the device, expand
    Channels
    , and then select an individual channel.
  2. In the
    Alarms
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal