Loading
Press Release | June 12, 2025

Rockwell Automation Helps Customers Unlock the Potential of Their Data with the Launch of OptixEdge

Advanced edge gateway solution transforms the way data is processed, enabling time and cost savings

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Allen-Bradley OptixEdge Advanced Edge Gateway, Right ViewKeep file name as is.

MILWAUKEE, Wis., June 9, 2025—Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and digital transformation, today announced the global launch of OptixEdge, an innovative edge gateway solution that revolutionizes data processing for industrial customers.

Today’s smart machines are generating more data than ever, but according to Rockwell’s latest State of Smart Manufacturing Report, only 44% of data is being used effectively. Many companies face challenges that prevent them from utilizing a vast amount of their data, such as network limitations, security concerns, or storage costs. Traditionally, data is sent to distant cloud servers to be processed, but this can be expensive and inefficient.

OptixEdge can directly address these issues by processing information where it’s created – at the machine, in real time. It connects to the user’s control system through Rockwell’s FactoryTalk® Optix™ software to collect, analyze, and send data to the cloud, enabling users to monitor and analyze machine or system data from multiple locations. This means faster insights, lower costs, and smarter decision-making.

"OptixEdge empowers customers to take control of their data like never before, providing powerful edge computing capabilities with flexibility, security, and ease of use,” said Jessica Morell, software product manager at Rockwell Automation. “By processing data at its source, OptixEdge enables customers to unlock valuable insights, improve efficiency, and drive innovation across their operations.”

Key capabilities of OptixEdge include:

  • Built-in Wizard App: A pre-installed FactoryTalk Optix application simplifies the data collection process and allows for easy configuration using only a web browser, cutting down on engineering time. It also offers the ability for users to build and deploy custom applications, if preferred.
  • Designed for efficiency: Allows lightweight applications to run in tandem with included software.
  • Secure remote access and troubleshooting: Remote assistance is available through FactoryTalk® Remote Access™, allowing remote engineers and maintenance teams to program, configure and troubleshoot systems over a secure VPN connection.
  • Open and flexible: OptixEdge can be utilized in conjunction with a plant or machine’s existing Rockwell hardware or third-party graphic terminals and controllers.
  • Cost savings and network performance improvement: OptixEdge offers users the ability to send less data to the cloud, which can help save money on storage and improve network performance.

Learn more about Rockwell’s innovative OptixEdge solution on Rockwell’s website.

Published June 12, 2025

About Rockwell Automation

 
 

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more productive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 26,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2025. To learn more about how we are bringing the Connected Enterprise® to life across industrial enterprises, visit www.rockwellautomation.com.


Media Contacts

Michelle Anderson
Michelle Anderson
Global Public Relations, Rockwell Automation
Connect:
EmailEmail

Topics: Hardware
Related News
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation Helps Customers Unlock the Potential of Their Data with the Launch of OptixEdge