MILWAUKEE—June 18, 2026— Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and digital transformation, today announced the availability of FactoryTalk® ResilientEdge™, a next-generation execution architecture designed to support autonomous manufacturing operations across highly-automated environments.
Built on FactoryTalk Optix™ and integrated across Rockwell Automation’s portfolio, including Plex Manufacturing Execution Systems (MES), FactoryTalk ResilientEdge creates a single execution layer that spans machines, people and production systems. The platform delivers predictable, low-latency execution at the edge along with cloud capabilities that enable analytics, Artificial Intelligence (AI) training and enterprise orchestration. The combination of edge and cloud means that operations are continuous even if connectivity is lost.
A Unified Execution Model
FactoryTalk ResilientEdge turns advanced manufacturing capabilities into a standard operating infrastructure by unifying plant models, connectivity, execution and intelligence into a single framework. Within FactoryTalk ResilientEdge, users will find a variety of innovative features: shared production model, native and interoperable connectivity, real-time edge execution with embedded business logic, cloud-scale analytics, and AI. The result is an execution system that eliminates the divide between Operational Technology (OT) and Information Technology (IT), dramatically reducing the complexity of deploying and evolving modern manufacturing operations.
“At a time when 95% of manufacturers are advancing AI and machine learning initiatives, FactoryTalk ResilientEdge enables a new class of manufacturing execution,” said Anthony Murphy, vice president of product management, Rockwell Automation. “Manufacturers can scale automation, intelligence, and autonomy across their operations while preserving the economic and scalability advantages of the cloud, helping manufacturers deploy faster and lower their total cost of ownership.”
Enabling AI-Driven Autonomy
Modern automation initiatives require reliable execution, structured data flow and scalable architecture as the foundation for advanced analytics and AI initiatives. FactoryTalk ResilientEdge delivers a resilient execution layer that supports advanced analytics, AI and closed-loop optimization without compromising plant-level performance.
Secure, Interoperable and Built to Scale
FactoryTalk ResilientEdge helps manufacturers modernize operations by improving operational resiliency, optimized for Rockwell Automation ecosystems while remaining open and interoperable across heterogeneous production environments. The security, interoperability and scalability of the new offering is a testament to Rockwell’s elastic MES solutions.
Faster Deployment and Lower Lifecycle Cost
By reducing integration complexity, centralizing monitoring and supporting modular scalability, FactoryTalk ResilientEdge can lower lifecycle costs and accelerate deployment. FactoryTalk ResilientEdge capabilities can be deployed as needed, supporting companies who phase their modernization strategy.
Representing a foundational shift in how manufacturers can scale execution systems, FactoryTalk ResilientEdge is available globally today.
Learn more about FactoryTalk ResilientEdge here.