Loading
Press Release | September 15, 2021
Recent ActivityRecent Activity

Rockwell Automation's Remanufacturing Program: A Sustainable Option for Productivity Savings

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
  • Main Image
  • Main Image

MILWAUKEE, September 15, 2021 /3BL Media/ - As defined by the Remanufacturing Industries Council, remanufacturing is a comprehensive and rigorous industrial process by which a previously sold, used, worn, or non-functional product is returned to a “like-new” condition, from both a quality and performance perspective, through a controlled, reproducible and sustainable process.

Not only does remanufacturing provide a cost productivity option for customers, it’s also good for the environment and supports the circular economy. It’s estimated remanufacturing saves, on average, 85% of energy, water, and material use compared to a newly manufactured product, according to The Association for Sustainable Manufacturing.

Rockwell’s global remanufacturing program uses the same high-quality parts, standards, and specifications as the original manufacturing process. Further, the company goes beyond just replacing components that have failed. Rockwell also provides firmware updates, proactively upgrades some components that have yet to fail, and tests them just like new products. 

Learn more about Rockwell Automation’s remanufacturing capabilities and how the company helps manufacturers worldwide meet sustainable production goals.

Published September 15, 2021


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation's Remanufacturing Program: A Sustainable Option for Productivity Savings