Rockwell Automation provides advanced automation technologies to help drive sustainability in a groundbreaking, zero-emissions vessel
MILWAUKEE - The world’s first vessel powered by hydrogen and renewable energy, the Energy Observer, is on a six-year trip around the world to prove a potential energy system of the future. Rockwell Automation has become an official supplier and service provider for this project, providing automation systems that help power the vessel, which operates with zero greenhouse gasses or fine-particle emissions.
To help ensure 24-hour energy autonomy throughout its global expedition, the Energy Observer uses a combination of intermittent renewable energy: solar panels, wind turbines, lithium-ion batteries and a hydrogen production system.
The Energy Observer team turned to Rockwell Automation for advanced automation technology to help control the vessel’s energy management system. The solution consists of an Allen-Bradley ControlLogix programmable automation controller, Allen-Bradley PowerFlex drives, Allen-Bradley POINT I/O, FactoryTalk View Site Edition (SE) supervision software and FactoryTalk Historian data-capture software, all of which integrate seamlessly to monitor and control the system. A central human machine interface (HMI) completes the solution, delivering real-time information to the crew.

Click to download image.
The energy management solution helps the Energy Observer team monitor, control and optimize the distribution of energy sources and make smart decisions about when and how to switch from one energy source to another. It also records the vessel’s operational data throughout its journey and communicates it back to the rest of the team on shore.
One example of this is the lithium-ion battery power being used to drive on-board systems like propulsion and desalination. Solar panels and wind turbines charge the batteries using PowerFlex drives. Should unfavorable environmental conditions cause the battery level to reach 30 percent or lower, the vessel’s hydrogen power source – fed from hydrogen created during the ocean water desalination process – activates to supply additional charging capabilities.
Representatives from the Energy Observer project were present in the Rockwell Automation booth at the recent Movin’ON World Summit on Sustainable Mobility presented by Michelin, held in Montreal in late May.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Kristen Crump
Rockwell Automation
414.382.0068
klcrump@ra.rockwell.com
Beatrice Zvosec
Padilla
612.455.1914
beatrice.zvosec@padillaco.com
Allen- Bradley, ControlLogix, FactoryTalk, Point I/O and PowerFlex are trademarks of Rockwell Automation Inc.
Published September 17, 2018