Loading
Blog
Recent ActivityRecent Activity

What’s Next for Industrial AI in Manufacturing?

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Executives and engineers reviewing production progress in a modern industrial facility, with advanced technology displayed on screens --chaos 40 --ar 16:9 --v 6.1 Job ID: 09b24edd-9623-4653-b68a-f3a8baaa210a

When I'm asked what excites me most about the future of industrial AI in manufacturing, two powerful shifts come to mind.

First is the variety of what’s now possible with modern AI. For years, valuable operational knowledge has been locked away in unstructured formats. This could include things like engineering notes, maintenance logs, procedures, incident reports, and decades of tribal knowledge.

Today, advances in language models allow manufacturers to finally access, interpret, and connect that information at scale. Think about a technician standing in front of a faulted piece of equipment at 2 a.m.. AI can surface the most relevant sections of complex equipment manuals, cross-reference production history, and deliver context-aware guidance at the moment it's needed. This changes how operators navigate troubleshooting and reduces the cost of being new to a problem.

The second shift is what’s happening at the edge. As intelligence moves out of centralized systems and closer to where work actually happens, manufacturers gain something they've never had before: the ability to deploy, update, and evolve AI-driven capabilities directly on the plant floor without long deployment cycles or rigid architectures. Models can be refined as conditions change, new use cases can be stood up faster, and the economics of innovation shift in favor of the plant rather than the IT roadmap.

Together, these advances dramatically compress time to value and enable AI to move from experimentation into real operational impact: safer operations, more resilient production, and continuous improvement.

Start with the Hard Problems

Every week brings a new headline, a new tool, or a new promise about how AI will transform the plant floor. Yet in conversations with manufacturing leaders, a familiar frustration keeps surfacing.  Despite the excitement, many AI initiatives stall, struggle to scale, or fail to deliver meaningful impact.

The most successful AI programs start in a very different place than the hype cycle. Instead of asking “What can AI do for us or what AI tool should we use?” they ask a more grounded question: “What operational problem are we trying to solve?”

One of the most common misconceptions I see is the belief that adopting AI means starting with the most advanced or fashionable technology available.

In reality, value comes from using AI as a means to an end, not as the end itself.

Manufacturers that see real results begin by identifying their toughest, most persistent challenges: recurring quality defects, unplanned downtime, inefficient changeovers, or slow root‑cause analysis. These are problems that already matter to the business. When AI is applied deliberately to these areas, it becomes a practical enabler of better decisions, not an abstract experiment.

Data Is the Real Differentiator

It’s important to remember that AI systems are only as effective as the data they rely on, and many organizations underestimate how foundational this step is. When operational data is fragmented, inconsistent, or poorly understood, even the most sophisticated models struggle to deliver reliable insights.

In practice, the manufacturers that move fastest are not always the ones with the most ambitious AI roadmaps. They are the ones with the most accessible, trusted, and contextualized data. The right approach is a parallel path: execute on use cases where data is already mature enough to deliver value, while simultaneously investing in the data foundation that will enable the next wave of capability. Early wins build confidence and momentum. Data improvement efforts build the runway. Both move together.

AI adoption becomes a progression, not a single leap, and organizations that understand this stop treating data readiness as a prerequisite and start treating it as part of the strategy itself.

Focus on Impact

AI discussions can quickly become theoretical. But on the plant floor, the organizations that sustain AI programs are the ones that define what success looks like before they build anything and create value that is tangible.

That means getting specific. Which metrics will move? OEE, first-pass yield, mean time to repair, changeover duration, defect escape rate.

  1. Pick the ones that reflect the problem you're solving and establish a baseline before you deploy.
  2. Build a rhythm for tracking and communicating results: not just to leadership, but to the operators and engineers living with the process every day.

When frontline teams can see that an AI application is reducing their troubleshooting time or flagging issues before they escalate, trust follows. Skepticism gives way not because you told people that AI works, but because they watched it work.

This focus on impact also helps organizations cut through noise. Instead of chasing every new AI capability, they invest in solutions that move the metrics that matter — and build the organizational credibility to tackle harder problems over time.

Making AI Practical on the Plant Floor

For AI to succeed in manufacturing, it must fit seamlessly into existing workflows. Solutions that demand radical changes in how people work often face resistance, regardless of their technical merit. The most effective AI applications are those that augment human expertise rather than replace it — surfacing insights at the right moment, helping teams prioritize actions, and supporting faster, more informed decisions.

When AI is designed with operators, engineers, and frontline teams in mind, adoption follows naturally. And as trust builds through visible results, metrics that move, and tools that genuinely reduce friction, organizations develop something more valuable than any single use case: the institutional confidence to keep going. That compounding effect, use case by use case, is how AI stops being a pilot program and starts becoming the way the plant runs.

Industrial AI
Industrial AI
Industrial AI
Industrial AI is powering the shift from industrial automation to autonomy. Learn how embedding AI into production systems transforms operational performance.
Learn More

Published June 9, 2026

Topics: Accelerate Digital Transformation Artificial intelligence Smart Manufacturing Industrial Automation & Control Digital Transformation

Chelsea Barnes
Chelsea Barnes
Director, Data Science & Digital Transformation, Kalypso

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left What’s Next for Industrial AI in Manufacturing?