Get the highlights
The state of cybersecurity in water utilities
As water systems become more connected, many utilities face growing risks, limited visibility, and increasing pressure to modernize securely.
30.5%
Of water utilities have fully identified all OT-networked assets.
30%
Of critical infrastructure providers have a formal cybersecurity plan in place.
12
Cyberattacks reported on 12 US water systems between November 2023 and April 2024.
"As the digital transformation accelerates within the water utility services industry, Rockwell Automation understands that the best practice for industrial security is a holistic approach that applies multiple physical and electronic defense layers across varying operational levels through well-defined policies and procedures.”
Ready to put these insights into action?
Our specialists are here to help you on the path to cyber resilience.