Create a complex dynamic link

Create a complex dynamic link by using the
Complex Dynamic Link Editor
to transform the value.
  1. In
    Project
    , select the variable that contains the property that you want the dynamic link to set.
  2. In
    Properties
    next to the property where you want to create the complex dynamic link, select  Add Dynamic Link.
  3. In the
    Dynamic link
    browser, select
    Advanced
    .
  4. In the
    Complex Dynamic Link Editor
    , select Add new and select:
    • Dynamic link
      and then specify the source to create a dynamic link.
    • A converter and then specify the source and converter logic to transform the value.
  5. Select the dynamic link direction to set the mode of the dynamic link. The direction changes as you select the icon:
    • Read from source node to the parent.
    • Write from the parent to the source node.
    • Read from the source node to the parent and write from the parent to the source node.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal