Create a ConveyorChassisMalfunction alarm trigger

Create a switch that triggers the ConveyorChassisMalfunction alarm.
  1. Create a switch that triggers the alarm:
    1. In the
      Project view
      pane, right-click
      MainWindow (type)
      and select
      New
      Base controls
      Switch
      .
    2. Hover-over the switch, select
      Edit
      , and enter
      TriggerConveyorChassisMalfunctionAlarm
      .
    3. In the
      Properties
      pane, create a dynamic link between the
      Active
      property and
      ProjectName
      Model
      ConveyorChassisMalfunctionAlarmVariable
      .
      For more information about dynamic links, see Create dynamic links.
  2. Create a trigger label:
    1. In the
      Project view
      pane, right-click
      MainWindow (type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      TriggerAlarmLabel
      .
    3. In the
      Properties
      pane, set the
      Text
      property value to
      Trigger the conveyor chassis malfunction alarm:
      .
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal