Local connection
The Local Connection mode allows for a local device connection to Runtime through a local network without logging on the
FTRA Manager
, nor accessing any server.The Local Connection mode is supported on devices where Runtime is installed, such as: HMIs and IPCs hosting Runtime, OptixPanels, routers, and Embedded Edge Compute modules.
NOTE:
To establish a Local Connection with OptixPanels
™
, routers, Embedded Edge Compute module, use their related System Manager. See the Local connection through Stratix
procedure further below in this chapter.®
4300 Routers and OptixPanels™
Once a Local Connection has been established, you can access
Interactive Access
. You can also set up any other connection type among those available in the section.
NOTE:
See Interactive Access applet for further information on this subject.
Local connection through Windows Runtime
To establish a Local Connection, proceed as follows:
- Start Windows Runtime.
- In the Windows Runtime pane, select theLocaltab and flag theEnable local connectionentry.
- Set a password to allow for later connection from your local device.
- Access theFactoryTalk Remote Access Tools Local Connectionfrom your local device..NOTE: TheFactoryTalk Remote Access Tools Local Connectionis automatically installed onto your device, when the Tools applets are installed. See Tools to learn more about how to download the Tools applets.
- A dialog box opens up. Enter the IP address or the device name and the password previously set in theTarget deviceandPasswordfields of the dialog box.
- You will be prompted to accept a certificate to establish a temporary o permanent secure connection.
- TheInteractive Accesswindow opens up.
Local connection through Stratix® 4300 Routers and OptixPanels™
®
4300 Routers and OptixPanels™
To establish a Local Connection, proceed as follows:
- Access the System Manager and selectFT Remote Accessfrom the main menu on the left.
- In theLocal Connectionsection, flag theEnabledentry.
- In the same section, set a password to allow for later connection from your local device. Click on theApplybutton.
- Access theFactoryTalk Remote Access Tools Local Connectionfrom your local device..NOTE: TheFactoryTalk Remote Access Tools Local Connectionis automatically installed onto your device, when the Tools applets are installed. See Tools to learn more about how to download the Tools applets.
- A dialog box opens up. Enter the IP address or the device name and the password previously set in theTarget deviceandPasswordfields of the dialog box.
- You will be prompted to accept a certificate to establish a temporary o permanent secure connection.
- TheInteractive Accesswindow opens up.
Provide Feedback