Profiles Access
Each profile grants a specified set of actions to a user account or group. There are four different types of profiles you can use for permission assignment:
Administration
, Network Security
, Device Installer
and Device Access
.
NOTE:
The
Administration
and Device access
profiles contain more granular permissions for further defining their permitted operations.Administration | It allows full control of the domain organization and log, and features more granular permissions to define the role. |
Network security | It allows full control of the firewall configuration. |
Device installer | It allows to associate devices to accessible domain and organization folders. |
Device access | It allows to perform remote device operations. |
Permissions are to be granted considering an appropriate level according to the user or group scope within the domain.
For example, grant Administration permissions at the root level to the organizational administrator. Grant Administration permissions at the folder level for site level administrators.
The
Administration
profile includes these permissions:Access users | It allows to view all of the user accounts defined for the folder. |
Manage users | It allows to create, edit, and delete user accounts and change user permissions. |
Manage folders | It allows to create, edit, move, and remove folders. |
View connection audit | It allows to access to the connections log. |
View operations audit | It allows to access to the administration log. |
The
Device Access
profile includes this permission:Network access (VPN) | VPN activation and subnetwork access; the sub network access can be additionally filtered by applying the firewall policies. |
Provide Feedback