Corrected anomalies in this release

The list identifies the anomalies corrected in
FactoryTalk Policy Manager
version
6.40.01 (CPR9, SR14)
.
Use the identification information provided in the brackets
[]
to track anomalies in future releases or to request assistance from Customer Support.
DTLS Timeout message displays indefinitely [1096593]
FactoryTalk Policy Manager
displays a warning when attempting to set the DTLS Timeout parameter for
FactoryTalk Linx
endpoints during deployment: The Studio5000 Engineering Station device does not support the DTLS timeout function.
FactoryTalk Policy Manager
displays the message indefinitely.
This anomaly first identified in version 6.20.
Cannot deploy configuration to Armor PowerFlex® devices [2042215]
FactoryTalk Policy Manager
cannot deploy policy model configuration to Armor PowerFlex® devices.
This anomaly first identified in version 6.30.
Cannot force resetting connections other than EtherNet/IP connections [1622662]
FactoryTalk Policy Manager
cannot force resetting connections other than EtherNet/IP connections. This prevents CIP Bridging policies from becoming effective immediately after a deployment.
TIP: To update CIP Bridging policies, reset the connections between nodes. You can do that by performing one of the following actions:
  • Power cycle the device
  • In case of a Logix controller, download an application
This anomaly first identified in version 6.30.
All chassis slots are allowed for outbound CIP bridging if you do not specify the chassis size [1655957]
If you do not specify the chassis size for a device, even with the
Disable Slots: All Slots
option selected, all slots are allowed for outbound CIP bridging.
This anomaly first identified in version 6.30.
Some devices may not have their configuration applied if Automatic Secured Device Replacement fails [1670977]
If the Automatic Secured Device Replacement process fails, some devices may not have their configuration applied.
TIP: To delete the impacted device configuration, you may need to factory reset the device.
This anomaly first identified in version 6.30.
Cannot deploy PSK to controllers [2020960]
If you attempt to deploy PSK to controllers (firmware revision 36.00,
FactoryTalk Policy Manager
displays this error
Unable to set a pre-shared key for Port
#
.
This anomaly first identified in version 6.30.
Improved certificates security
Improved the security of certificate generation process.
This anomaly first identified in version 6.40.00.
Improved backups security
Improved the security of backup temporary files.
This anomaly first identified in version 6.40.00.
Improved PSK security
Improved the security of pre-shared keys (PSK).
This anomaly first identified in version 6.40.00.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal