Develop filterable data grids

Develop a grid that displays motor parameters and a grid that display motor manufacturing details.
Application example
NOTE:
Download a sample project:
FilterableDataGrids.zip
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
TIP: For examples on how to filter motor parameters with queries, see Numeric data query examples.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.