Tooltip style
Style for tooltips
Properties
Name | BrowseName | DataType | Description |
|---|---|---|---|
Background color | BackgroundColor | If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property | |
Provide Feedback