Switch style

Style for switches
BrowseName
SwitchStyle
SuperType
Control style(ControlStyle)

Properties

Name
BrowseName
DataType
Description
Background color
BackgroundColor
If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property
Border color
BorderColor
Color of the polygon border
Border width
BorderWidth
Thickness of the object border
Text color
TextColor
Color of the text to display
Font family
FontFamily
Font family
Font weight
FontWeight
Font weight
Font italic
FontItalic
Enables/disables italics in the text
Font size
FontSize
Font size
Active background color
ActiveBackgroundColor
Background color of the element while is active
Active border color
ActiveBorderColor
Border color of the element while is active
Active text color
ActiveTextColor
Text color of the element while is active
Handle color
HandleColor
Color of the element's handle
Handle border color
HandleBorderColor
Color of the handle border
Handle border width
HandleBorderWidth
Width of the handle border
Radius
Radius
Radius of the angles of the objects
Focus border color
FocusBorderColor
Border color of the element while is being selected
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal