Date and time

Display DateTime data
BrowseName
DateTimePicker
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Value
Value
Value displayed and possibly changed by the user
Font family
FontFamily
Font family
Font weight
FontWeight
Font weight
Font italic
FontItalic
Enables/disables italics in the text
Font size
FontSize
Font size
Text color
TextColor
Color of the text to display
Control in read-only mode
ReadOnly
Enables/disables the read-only mode. If enabled, it is not possible to write in the text box but. For example, it is possible to select the existing text for copy-paste
Text horizontal alignment
TextHorizontalAlignment
Indicates where the text is positioned on the horizontal axis
Text vertical alignment
TextVerticalAlignment
Indicates where the text is positioned on the vertical axis
Border color
BorderColor
Color of the polygon border
Input format
InputFormat
Date and time with seconds (default) shows date and time in extended form. Date and time without seconds shows date and time without seconds. Date shows the Date without any time. Time with seconds shows the Time (including seconds. Time without seconds: Shows only hours and minutes
Style
Style
Graphic style applied to the control
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

Modified value
BrowseName
Event that is triggered when the user changes the value of the control
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal