Text trimming
How to trim text if is longer than the control
- BrowseName
- ElideEnum
Values
Value | DisplayName | Description |
|---|---|---|
0 | None | No trimming is performed |
1 | Left | Only the last part (ending) of the string is displayed |
2 | Middle | Only the central part of the string is displayed |
3 | Right | Only the left side (beginning) of the string is displayed |
Provide Feedback