System

Enables read/write at runtime for some system settings of the network interfaces.
BrowseName
System
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Reboot required
RebootRequired
Requires a device reboot to commit system configuration changes
Network interfaces
NetworkInterfaces
List of the network interfaces.
Date and time
DateAndTime
Date and time configuration.
Device
Device
Device status and configuration.
Display
Display
Device display status and configuration.
Application
Application
Application status and configuration.

Methods

Reboot
BrowseName
Reboot
Restart the system. For supported operating systems, verify if the user running the FactoryTalk Optix Application has the authorization to perform the operating system restart.
Load application
BrowseName
LoadApplication
Load application onto device
InputArguments
Name
DataType
Description
FilePath
FilePath
Password
Password
DeleteApplicationFiles
DeleteApplicationFiles
OutputArguments
Name
DataType
Description
Result
LoadApplicationResult

Events

LoadApplicationStatusEvent
LoadApplicationStatusEvent
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal