OMRON EtherNet/IP station

BrowseName
OmronEthernetIPStation
SuperType
Communication station(CommunicationStation)

Properties

Name
BrowseName
DataType
Description
Maximum job size in bytes
MaximumJobSizeInBytes
Maximum size of a transmission of tags from the controller (in bytes). 0 = 504 bytes (maximum value).
IP address
IPAddress
Unique address of the controller on the network
Port
Port
Number of the port used by the TCP-IP connection. It must match the one configured in the controller.
Timeout
Timeout
Maximum wait time in milliseconds to receive a response from the controller.
CPU slot
CpuSlot
Number of the slot occupied by the CPU in the controller rack.
Operation code
OperationCode
(Inherited from Communication station)
Tags
Tags
(Inherited from Communication station)
Types
Types
(Inherited from Communication station)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal