Trend
View the trend of the values of one or more variables read in real time and/or logged.
Properties
Name | BrowseName | DataType | Description |
|---|---|---|---|
Query | Query | Standard SQL query to filter the data of interest. You can use it to filter data from a database and to filter data obtained from a node-based model. In case of a node-based model, the SELECT * FROM Model part is mandatory, followed by the WHERE clause with which to indicate the search conditions - for example: SELECT * FROM Model WHERE Speed > 40 | |
Reference time zone | ReferenceTimeZone | Time zone for displaying the date and time on the X axis. (UTC: time zone standard; Locale: time zone of the device from which the data is generated; Session: session time zone). To record the data displayed in local time zone, enable the Local Time Log property of the Data logger object. | |
Pen X axis | XAxis | The X axis for the trend pen, that shows the time being measured. Can be set to automatically scroll forward in time during runtime by setting the Follow property to True. | |
Pen Y axis | YAxis | The Y axis for the trend pen, that shows the value of the variable being measured. Use the default Y axis values or set the properties to define minimum and maximum values. Can be set to automatically scale at runtime to resize the trend graph according the the values being displayed. | |
Methods
Refresh
- BrowseName
- Refresh
Provide Feedback