Create a variable type

Create a variable type to be able to create variables of the type and add those variables to object.
  • From
    Project view
    , drag an existing variable into a folder in
    Type view
    . The type appears in both
    Type
    view
    and in the
    Project
    view
    folder that has the same name as the folder in
    Type
    view
    .
TIP: The variable in
Project
view
is appended with
(type)
and the original variable that you dragged from
Project
view
is now an instance of the type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.