Synchronize the imported tags

Synchronize imported tags to update their data types, names, and structures.
  1. In
    Project view
    , navigate to the
    TagImporter
    object associated with a
    Communication station
    object.
  2. Double-click the
    TagImporter
    object.
    The editor shows the status of each controller tag in the
    FactoryTalk Optix Studio
    project.
  3. Select
    Apply
    to complete the synchronization of imported tags.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.