Type view

Types are models of objects or variables from which other objects and variables are created. Use
Type
view
to add an object type to the editor to create an instance of that type. Drag the type from a folder in
Types view
to the window or canvas.
Types are organized into folders by category of object. Example folders include types for the user interface, databases, loggers, alarms, and recipes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.