Event types
FactoryTalk Optix Studio
projects include predefined events and may include custom events.Predefined events
Some objects contain predefined events. For example, a
Button
object contains a predefined MouseClick event
that triggers an associated method when you click the button at runtime.The
Events
pane lists the predefined events for an object.Custom events
Custom events include configurable change events that occur at runtime when the value of a variable changes. For more information, see:
Provide Feedback