Web presentation engine
When a client connects at runtime to the specified web server URL, generate an interactive session for the authenticated user.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Dynamic variables polling time | DynamicVariablesPollingTime | Time interval for the periodic reading of the dynamic link source field variables. | |
Protocol | Protocol | Protocol used for communication between web clients and the server, either https or http. | |
IP address | IPAddress | Server IP address. If you host the server locally, set its IP address to "127.0.0.1". Do not use the "localhost" keyword and do not include the protocol information ("http://", "https://") before the IP address. | |
Maximum number of connections | MaxNumberOfConnections | Maximum number of clients that can connect to the web server. | |
Provide Feedback