Switch style

Global properties for all project Switch objects.
BrowseName
SwitchStyle
SuperType
Control style(ControlStyle)

Properties

Name
BrowseName
DataType
Description
Background color
BackgroundColor
If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property.
Border color
BorderColor
Color of the polygon border.
Border width
BorderWidth
Thickness of the object border.
Text color
TextColor
Color of the text to display.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Active background color
ActiveBackgroundColor
Active border color
ActiveBorderColor
Active text color
ActiveTextColor
Handle color
HandleColor
Handle border color
HandleBorderColor
Handle border width
HandleBorderWidth
Radius
Radius
Radius of the angles of the objects.
Focus border color
FocusBorderColor
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.