Navigation panel style

Global properties for all project Navigation panel objects.
BrowseName
NavigationPanelStyle
SuperType
Control style(ControlStyle)

Properties

Name
BrowseName
DataType
Description
Color
InactiveColor
Color of the range.
Inactive text color
InactiveTextColor
Active color
ActiveColor
Active text color
ActiveTextColor
Background color
BackgroundColor
If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Radius
Radius
Radius of the angles of the objects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.