Navigation panel item

Panel that can be displayed in a navigation panel object.
BrowseName
NavigationPanelItem
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Title
Title
Panel title, to be displayed in the navigation tab of a Navigation panel object. If not set, the panel BrowseName is displayed.
Image path
ImagePath
Image to be displayed in the navigation tab of a Navigation panel object. The image overrides the panel Title or BrowseName. For seamless integration with the UI, use correctly sized flat images with a transparent background.
Panel
Panel
Panel to be displayed. Must be a widget.
Panel alias node
AliasNode
Node to which to point any alias in the panel to be displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.