Data grid column

Data grid object column.
BrowseName
DataGridColumn
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Title
Title
Panel title, to be displayed in the navigation tab of a Navigation panel object. If not set, the panel BrowseName is displayed.
Width
Width
Width of the window. It can assume values greater than or equal to zero. The Auto value sets the width equal to the width of the content (in this case, in the absence of content the object collapses).
Header alignment
HeaderAlignment
Horizontal alignment of the content in the header row.
Content alignment
ContentAlignment
Horizontal alignment of the content in the rows other than the header row.
Order by
OrderBy
Attribute/property of the nodes or column of a table by which to sort the elements. Generally the same attribute/property or column from which the elements are obtained is set.
Data item template
DataItemTemplate
Data item template object which can contain data in textual or image format.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.