Horizontal alignment

Alignment of the object on the horizontal axis.
BrowseName
HorizontalAlignment

Values

Value
DisplayName
Description
0
Left
The left side is positioned on the left side of the container, except for the left margin.
1
Right
The right side is positioned on the right side of the container, except for the right margin.
2
Center
The center of the object is positioned in the center of the container, except for the left and/or right margins.
3
Stretch
object width equals container width, except for the left and/or right margins.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.