OPC UA server

Publishes nodes of the information model for the OPC UA client project.
BrowseName
OPCUAServer
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Endpoint URL
EndpointURL
Communications protocol and network address of the endpoint on the server.
Sampling interval
SamplingInterval
Time interval between successive readings of the field variables by the server.
Maximum number of connections
MaxNumberOfConnections
Maximum number of OPC UA clients that can connect to the OPC UA server.
Minimum message security mode
MinimumMessageSecurityMode
Minimum security level for messages exchanged between client and server. None = the messages can be unsigned and unencrypted; Signature = the messages must be signed or signed and encrypted; Signature and encryption = the messages must be signed and encrypted.
Minimum security policy
MinimumSecurityPolicy
Minimum security level for messages exchanged between client and server. None = the client does not require any specific security policy; Basic256Sha256 = this policy or more secure; Aes128_Sha256_RsaOaep = this policy or more secure; Aes256_Sha256_RsaPss = this policy.
Server certificate file
ServerCertificateFile
Server public certificate file, according to standard X509v3 and with .der extension. It must be found in the FTOptixApplication/ProjectFiles/PKI/Own/Certs folder. If specified, the private key must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certs folder.
Server private key file
ServerPrivateKeyFile
Server private key file, with ASCII Base64 encoding and .pem extension. It must be found in the FTOptixApplication/ProjectFiles/PKI/Own/Certs folder. If specified, the certificate must also be specified. If not specified, it is automatically generated at runtime in the FTOptixApplication/ApplicationFiles/PKI/Own/Certs folder.
Product URI
ProductURI
URI that globally identifies the software.
Product name
ProductName
Name of the software.
Manufacturer name
ManufacturerName
Name of the software manufacturer.
Nodes to publish
NodesToPublish
Configuration of the nodes to be published and the users to publish them to.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.