What's New
Current Release
1.00.02 - Dec 2023Fixed Anomalies
Fixed Anomalies
- Users encountering an authorization error while attempting to add meters or browse tags, resulting in an error message being displayed (3183023).
- Refresh Issue while switching to other Organizations/Tenants for the users with multi-organization access (2346392).
Known Anomalies
Known Anomalies
- The duplication of months observed in the yearly bar graph representing Consumption/Production data for Resource Meter and Production Meter (2257140).
- Issue with the proper display of the heatmap for energy consumption, specifically related to the month and year granularity (2338177).
- On month selection in dashboard charts, the past month's value is not displaying correctly (2292724).
- The cost is not being displayed according to the new site currency when moving a node/meter from a site with a different currency (2284513).
- The node is not getting greyed out on the base/configuration details selection (2229785).
- The child nodes are getting displayed multiple times upon clicking the enterprise node (2320812).
- The widget Duplication at Site Level & Total cost detailed widget is missing (3141590).
- Clicking the Notifications icon from the left-side navigation menu is causing the page to load indefinitely (3160726).
- Issue with the "DAY" filter for the heatmap chart where the minute interval values of 45 and 60 are not being displayed (3163431).
- Issue with the Energy Consumption and Total Consumption-Production Data chart where Natural Gas data is not displaying correctly for the selected month (3202997).
Provide Feedback