Related Documents

Select the specific guides for the operating system and purpose.
DataView Installation Guides
There are two types of installation guides: Installer and Advanced Installation.
  • Installer
    This guide will instruct an experienced IT administrator to follow the installer step by step to install the application. Use this guide and the executable application file to install the application.
    The installer will unzip the files, which allow the administrator to accept the license agreement and install the application based on the selections:
    NOTE:
    For first time installation and testing, using the installer version is a recommended starting point.
  • Advanced Installation
    This guide will instruct an experienced IT administrator to follow the installer step by step to install the application. This method allows the administrator to manage a customized installation. This Installer will unzip the files and allows the administrator to accept the license agreement.
    • 4.01.00_FactoryTalk Analytics DataView Advanced Installation Guide (Windows)
Security Installation Guide
This guide is used in conjunction with the Advanced Installation Guides. It will instruct an experienced IT administrator step by step how and when to install the Security Provider:
  • 4.00.00_Analytics Security Provider Advanced Installation Guide (Windows)
FT Activation Service Installation Guide
This guide is used in conjunction with the Advanced Installation Guide. It will instruct an experienced IT administrator step by step how and when to install the FactoryTalk Analytics Activation Service:
  • 2.1.1_FactoryTalk Analytics Activation Service Installation and Configuration Guide for 4.01.00 DataView
InfoPlatform Installation Guide
This guide is used in conjunction with the Advanced Installation Guides and Installer Guides. It will instruct an experienced IT administrator step by step how and when to install the InfoPlatform:
  • 4.00.00_FactoryTalk Analytics InfoPlatform Service Installation and Configuration Guide
User Guides
These guides will provide the User Interface and configuration information after installation is completed and provide the steps on how to use the features offered in the application.
  • 4.01.00_FactoryTalk Analytics DataView User Guide
  • 4.01.00_FactoryTalk Analytics DataView Connectors Configuration Guide
  • 4.01.00_FactoryTalk Analytics DataView Administration Guide
  • 4.00.00_Analytics Security Provider Administration Guide
IMPORTANT:
The images in these guides are provided as examples. They may not match the version being installed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal