Export Hierarchy

Perform the following steps to export hierarchy:
  1. Click on the [] icon from the Enterprise in the hierarchy list and select [Export Hierarchy].
    Select export hierarchy
  2. In the pop-up window, provide the file name and select the location to export.
  3. Click [Save].
    Select location
    The "
    Enterprise.xml exported successfully
    " message displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal